Hi,
We are a slave device in a CAN-bus network, sometimes when the master shuts off the bus network, then the voltages on CAN-H/L will go up to 40V and remains there, because for that reason we want to use the ISO1044 because the CAN-bus pins might go up to 40V in certain conditions.
So we were thinking, if we connect both GND's together and both VCC's, so that they work on our GND and VCC that is also used by our microcontroller, will the 40V protection on CAN-H/L still work?
Or is there a better solution to protect us from this. We only have our main power and cannot use external power from the master to feed the other side of the CAN-isolator (we only have GND coming from the master). so somehow we need to generate this power on our own.
Best regards,
Jan