This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1212: unused pin

Part Number: ISO1212

How to deal with the unused pin as Pin6 and Pin7? Powering it to VCC1 or GND1. Which method is better for noise immunity?

Regards

Brian W

  • Hi Brian,

    Pins 6 and 7 are not connected internally, hence, it shouldn't matter whether these pins are connected to VCC, GND or left OPEN. If leaving them OPEN is okay for customer then you can ask them to do so. Thanks.

    Regards,
    Koteshwar Rao