This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6741: VCC1/2 range

Part Number: ISO6741

Hello,

I have a question for VCC1/2 range of ISO6741.

According to the datasheet, both VCC1 and VCC2 has two different ranges, 1.71-1.89V and 2.25-5.5V.
Does it mean it doesn't support 1.89V-2.25V range? Why don't you specify simply 1.71-5.5V?

Regards,
Oba