Part Number: ISO1430
Other Parts Discussed in Thread: THVD1450
Hello team,
Here is the questions from our customer.
- ISO1430 has failsafe function.
The failsafe function is only for receiver and it couldn’t contribute to the receiver of other device they use SN75176.
Is it correct ? - In case that DE of ISO1430 is L or unknown, the driver output should be Hi-Z so the bus will be idle if driver of SN75176 is Hi-Z as well.
- Or Does ISO1430 have the function to prevent the bus idle even if the other driver or ISO1430 output is Hi-Z sate ?
<Background>
- Our customer has two equipment and one is implemented ISO1430 and the other is SN75176.
- They are considering replace SN75176 to SN65HVD178 to prevent the fail communication during bus idle.
- In their understanding, question 1 and 2 is yes but question 3 is no but they would like to double check.
Thank you and best regards,
Michiaki