This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6721: About internal circuit

Guru 11170 points

Part Number: ISO6721

Hello E2E,

How many transistors included in the device?

Best regards,
ACGUY

  • Hi ACGUY,

    Thanks for posting your question.

    Unfortunately, this is TI proprietary information that is not available to customers.

    However, device reliability information, such as Mean Time Between Fails (MTBF) and Failures in Time (FIT) rates are available from ti.com device product folder in the Ordering & quality tab. Direct link is here. Please note that ISO6721 is in Preview status and some of the quality information will be populated when the device is in full production.

    Regards,

    Dushmantha