Part Number: ISO7742
Dear Team,
My customer would like to use ISO7742FDWR in two different scenarios :
1. Vcci=3.3V ; Vcco=5V
2. Vcci=5V ; Vcco=3.3V
As a result our questions are :
1. Is it allowed work with different voltages on Vcci/Vcco ? (Datasheet demonstrates only cases where Vcci=Vcco)
2. Are there any additional considerations on which of the Vcc1/Vcc2 should be the higher/lower voltages
Best regards,
Nir