Part Number: SN6505A
Other Parts Discussed in Thread: SN6505B,
Hi Sir,
May we know that SN650x series can input +5V and output -5V isolation application?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tommy,
Since SN6505A or SN6505B based solution generates an isolated output, the output GND reference is completely isolated from the input. Hence, if you consider the negative terminal as reference point, the the positive terminal is going to be +5V. Similarly, if you consider the positive terminal as reference point, the negative terminal is going to be -5V. This is true for all isolated power supply solutions.
Please see below image for a pictorial explanation, thanks.
Regards,
Koteshwar Rao