Part Number: ISO7742
Other Parts Discussed in Thread: ISO6741
Hello;
I have a design that requires some isolations; details are described as below.
1. An UART interface (RX/TX signals, baud rate up to 1Mbit/s) and another digital sync signal X (switching at 1MHz, irrelevant to UART) , these signals need to be connected to another PCB which has completely different a power domain. Which isolation device would you recommend?
2. An USB port will be connected to a PC. Which isolation device would you recommend?
Thank you very much!
Wen Li