Part Number: SN6505B
Other Parts Discussed in Thread: SN6505A
Hello,
I am using SN6505B along with 750316818 (5V to 15V/390mA). I am looking for alternatives that can provide 3KV reinforced isolation and better V/us. I came across the following options.
- PH9185.013NL https://products.pulseelex.com/product-details/pm2190.013nl/2819/
- PH9385.013NL https://productfinder.pulseeng.com/product/PH9385.013NL
1) Please help by reviewing the options and let me know if there is any concern using one of these with SN6505B.
2) Any concerns with regulating the output using Switching Buck converter (TPS560430XDBVR) instead of an LDO? The 15V output is being regulated to 12V (for gate drives) using an LDO and to 3.3V using TPS560430XDBVR (for control circuit). The LDO and Buck both connect to the transformer output.
3) SN6505B can only handle 5V maximum input voltage. Any other options that can take 12V or 15V input? The 5V max input limit is forcing me to the following topology:
400VDC INPUT > 15VDC (UCC28881D) > 5VDC (TPS560430X) > [SN6505B + 1:3.5 TR = 15V ISO] > [12V LDO || 3.3V Buck]
The efficiency is being lost in the conversions.
Regards,
WB