Other Parts Discussed in Thread: THS4081
Manuel
Looking for an SOT-89 pkg LDO that can handle 12-15 V input, give 5.2v output to drive SN6505 which has multiple isolated outputs? The total current from 5.2V running the SN6505 is <100mA
Also: is there a TI part for charge pump converting 5.2V to -5V? Output current <3,A for THS4081 VSS supply.
robin