Part Number: ISO1050
Dear sir/madam,
I have been working on a CAN connection while using a PIC18F27Q84 with build in CAN controller and the ISO1050 isolated CAN transceiver.
When I programmed the pic it sends out a signal to the ISO1050, but the CAN output of the ISO1050 is incorrect.
Here is a picture of it. The purple signal is the TX input of the ISO1050. The yellow signal is the CANH and purple signal the CANL.

The voltage is always at 0V instead of the normal 2.5V and the CANH and CANL are not inverted from eachother. Also the recessive and dominant voltage are not correct.

This is the circuit and R26 is the 120 ohm resistor for the CAN.
Any idea where I went wrong?