Part Number: ISOW7840
Other Parts Discussed in Thread: ISO7840, ISO7740, ISO6740, ISO7741
Hi,
I would like to use the isow7840 digital isolator to drive with an FPGA, the synchronization lines of four hydrophones submerged in water. The hydrophones are powered by an external DC/DC converter so I don't use the isolated dc/dc power from the chip. If water enters in one hydrophone, its line could short out to ground but our system can switch off each single hidrophone. The iso7840 guarantees that the short circuit does not propagate towards the FPGA but what happens to the other working output lines? Could they short out to ground too? Thank you. Regards, Emanuele Giacomozzi