Hi Team,
My customer is surveying ISO1212 and has few questions as following, please help to provide comments.
1. May I said that the tolerance of SENSE pin is 6.5V for VIL(min) and 8.55 for VIH(max), right?

2. If the answer for Q1 is yes, the equation of VIH(max) should be 8.55V+1kohm*2.25mA*562ohm/562ohm ( use1kohm resistor as Rthr, 562ohm resistor as Rsense), right? Then the calculation result of VIH(max) is 10.8V but datasheet shows the VIH(max) is 10.95V. Please correct me if my understanding is wrong.
3. If Rthr is 0ohm, the calculation result of VIL(typ) is 7.1V, VIH(typ) is 8.25V, the result is different to the values shown in above table. Why?


4. Is there a same chart like below but the Rthr is 1kohm?

Thanks a lot.
Vincent Chen


2. Customer tested EVM(RTHR is 1kohm, RSENSE is 562ohm), when applying 5V on pin9 of J4. The current flow into RTHR is about 1.45mA. Is this value expected? That is why customer asks input current plot with 1kohm RTHR.