Part Number: ISO7041
I am an IS consultant working on a complex IS design and had planned on using the isolator clauses in the IEC 60079-11 standard for a serial IS interface.
I was thrilled to find that TI has achieved this certification.
I have obtained the IEC and ATEX certificates from your web site.
However, there is a confusing detail.
Section "7.8 Safety Limiting Values" of the data sheet would tend to imply the TOTAL POWER for the part is 1.435 watts and de-rated accordingly. I have always assumed this meant total, as in total between both sides. However, the IEC certificate and ATEX certificate both say 1.3 watts each side for 70C and 1.1W each side for 85C. No matter how you add it up, that does not make sense.
The Intrinsic safety standard is always more conservative, and would also requite a 1.5 safety factor. SO even if testing improved the certification, I cannot imagine it flew by without the 1.5 safety factor on top of it.
I need more particulars and I am certain this will need to come from the person who handled the certification, as very few people are well versed in Intrinsic safety and it is a language all of its own.
Please either get me the full certification test report or please connect me directly with the person who handled the certification.
I already have the certificates. That is not enough info. I have also read your "Application Report SLLA480–May 2020 Intrinsic Safety Compliance of Digital Isolators in Explosive Atmospheres" whichj also is not useful for real design work.
Thanks
Glen E Schmidt
AnalogIS LLC
Analog Design + Intrinsic Safety = AnalogIS
A UNIQUE COMBINATION OF TWO OF THE MOST DIFFICULT SKILLS TO FIND IN THE INDUSTRY
2513 Centre Rd
Bartlesville, OK 74003
glen@analogIS.net