Hello guys,
I'm planning to use the TL760M33 3.3 LDO voltage regulator and I'm concerned about the stability of the IC with respect to the output capacitor ESR. Datasheet says the ESR should be between 1.4 and 2 Ohm.
The thing is that I'm using, in the 3.3V power bus, some low ESR caps to filter EMI. Will theses caps destabilize the LDO, even if they are not close to it? If so, how can I solve the problem?
Thanks in advance,
André.