This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354 Power Estimation for 720MHz (Max Frequency)

Other Parts Discussed in Thread: AM3354

Hi,

Power estimation report for AM3554 processor operated at 576MHz frequency is given in the table below (As received from TI using power estimation tool "PET").

Kindly let me know the relative  power consumption for AM3354 processor  operated at 720MHz (Max) frequency.

AM335x Power Estimation Report
Input File Name: am335x_pet_input_adv.xls
Junction Temperature (°C): 25
Device Process: nominal
ARM Clock Freq [MHz] 720.0
  Voltage   Leakage Active Total  
  Current (A)         Power (W)
  min max average      
VDD_MPU 1.26 1.26 0.002 0.391 0.392 0.49451
VDD_CORE 1.10 1.10 0.002 0.310 0.312 0.34320
VDDS_DPLL 1.80 1.80 0.000 0.009 0.009 0.01663
VDDS_SRAM 1.80 1.80 0.005 0.000 0.005 0.00910
VDDS_DDR 1.80 1.80 0.000 0.070 0.070 0.12633
VDDS_1P8 1.80 1.80 0.000 0.004 0.004 0.00695
VDDS_3P3 3.30 3.30 0.000 0.005 0.005 0.01776
VDDA1P8V_USB0/1, VDDA_ADC 1.80 1.80 0.000 0.000 0.000 0.00000
VDDA3P3V_USB0/1 3.30 3.30 0.000 0.000 0.000 0.00000
Total           1.01449
Notes : 
VDDS_DPLL includes VDDS_PLL_MPU, VDDS_PLL_CORE_LCD and VDDS_PLL_DDR power supplies
VDDS_SRAM includes VDDS_SRAM_CORE_BG and VDDS_SRAM_MPU_BB powre supplies
VDDS_1P8 includes VDDS, VDDS_RTC, VDDS_OSC and 1.8 V VDDSHVx power supplies
VDDS_3P3 includes 3.3 V VDDSHVx power supplies

Calculated maximum module utilization for the selected OPP
Module Slot 0 Slot 0 Unit
Max Current
Cortex A8 720 576 MHz
SGX 1600 1280 MBps
EDMA 800 640 MBps
EMIF 3200 2560 MBps
GPMC 800 640 MBps
OCMC-RAM 800 720 MBps
LCDC 800 760 MBps
USB 800 480 MBps
Ethernet MAC 800 0 MBps
PRUSS 800 0 MBps
MCASP1 800 560 MBps
MCASP2 800 0 MBps
MMC1 800 640 MBps
MMC2 800 640 MBps
MMC3 800 640 MBps
misc. 6800 1080 MBps

Regards,

Sarusha Narayan