I would like to confirm the current protection of TPS65320-Q1.
The threshold of the current protection is 4A(min.) and 6A(typ.) in the datasheet.
When the current is over the threshold (ex short), the protection is active.
After the protection is active, the condition comes back normal.
In this case, can the converter operate come back normal operation automatically?
Best regards,
Atsushi Yamauchi