The specification sheet says that short circuit protection is included for added Vout and 5Vg at page12. However, I couldn't find specifed threshold voltage of this in the sheet. So, I evaluated EVM and found that it continued switching function when Vout=0V and Vin>5V, stopped it when Vout=0V and Vin<5V. Then, what is the definition of this short circuit protection?