Hello Team
My customer evaluate TLV62065 for DDR3 power supply.
they measured near 40mV transient at referense LC in 1P of datasheet.
They confirmed that It could satisfy target of load transient when changing L=0.47uH or C=100uH.
These values seems not recommended in data sheet and Webench(TPS62065) , will it have a problem to use with these values?
【Condition】
・Vin 5V
・Vout 1.35V
・Iout 0.1A→0.8A
・PWM mode
・Target within 30mV transient
Regards
Tomohiro Nagasawa