This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A6350-Q1 enable pin



Dear All

 

In datasheet, Device enable input voltage is 0 to 0.8V at low level and 2.5 to 40V at high level.

if Enable voltage is between 0.8 and 2.5V, is TPS7A6350  enable or disable ?

 

Best regards.

 

 

  • Hi Mike,

    EN is logic pin. When EN voltage between 0 and 0.8V, device is disable. When EN voltage between 2.5V and 40V, device is enable.
    If EN voltage is between 0.8 and 2.5V, device working status is uncertain.
    So please make sure the EN voltage is below 0.8V or above 2.5V (<40V) to get the certain working status.

    Best regards,
    Jason Liu