Hi,
I want to know two things about this IC:
1. is it ok to connect VCC to 5V and S0-S3 to signals at 3.3V?
2. Is it ok to drive a solenoid of 62ohm & 5V rating through this device where i/p is connected to 5V and o/p to solenoid (as On resistance is 70 ohm and max current rating is 50mA)?
Regards
Srikanth