Other Parts Discussed in Thread: TPS65381-Q1
Hi,
This is about the device behavior under Slow VBAT ramp-up/down.
Currently our application uses TPS65381-Q1 with TMS570LS071x.
We found an application report (SLVA643) which mentions the device
behavior with slow ramp-down/up conditions, but we couldn't understand
what measures should be taken for the Slow VBAT conditions.
Is it necessary to consider Voltage Supervisor IC for VBAT?
This E2E mentions that "if this rising edge is slow, i.e. 300ms, the TPS device will release
the reset before VBAT gets to 5.8V (the min voltage to operate for TPS65381),
and then cause a TPS65381 BIST test failure. Eventually, you will find your
TPS device staying in safe state."
What should be done if the device goes into the Safe state? please let us
know the procedure to change the device from Safe state to Reset or standby state.
Best Regards
Kummi