Hi team,
I am reviewing the Output Pulse Width provided by CD74HC4538-Q1 for below configurations.
The datasheet contains the K factor and time constant for few combinations. Unfortunately it doesn't cover the design values I'm using.
VCC varies between 4.9V to 5.1V
Operating Temperature range -40°C to 125°C
Scenario -1: Rx=100k Cx=1uF
And
Scenario -2: Rx=150k Cx=10uF
Can you please provide the K value for my specific conditions?
Also, is it possible to obtain a SPICE model that can run on SIMetrix simulation tool?
Thank you,
Jared