This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65310EVM / Working without GUI

Hi,

I can't work customeed TPS65310EVM without GUI.

Current TPS65310EVM conditions are followings;

- LDO is not used. The VSENSE4 is tied with GND

- Jumpers are set same as Table 4. EVM Jumper for Operation Without Using USB Interface and GUI Software

Can the TPS65310EVM work without conncting VBUS(CON17)?

Best Regards,

Kuramochi