I have a camera that produces a square wave with varying wave duration(width) every time the cameras shutter triggers. I also have a 24V 1A DC power supply, and two LEDs that need approximately 27.5V at 430mA DC. I am looking for a device that would receive a specific signal width from the camera then it triggers LED 1 at the predefined current for a time duration, and then receive another signal with a different width from the camera at the same channel and will trigger LED 2 at the predefined current for a duration. Is the a devise like that? How would I go about making something like this?
Thanks.