Hi all
Would you mind if we ask UCC28950-Q1?
<Question1>
About Master and Slave mode formula from (15) to (19) on the datasheet, our customer uses one circuit.(there is no slave)
In this case, they had better use (15), (17) and (19), right?
When they would like to use slave mode, is the setting as follows?
-The setting-
To set the converter in slave mode, connect the external resistor RT between the RT pin and GND, and place an 825-kΩ resistor from the SS pin to GND in parallel to the SS_EN capacitor. This configures the controller as a slave.
<Question2>
On the formula (15), there is "Ids(master)=(-25×(1-D)+5)uA".
Duty is maximum 97%.
In case of D > 0.8, the value of Ids(master) will be plus value.
Does it mean that CSS is not discharged? Otherwise, is it charged?
If it is charged, the voltage of SS pin does not decrease, does the switching keep on?
We need your help.
Kind regards,
Hirotaka Matsumoto