This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

transducer that is usable with PGA450Q1EVM

Guru 29720 points
Other Parts Discussed in Thread: PGA450Q1EVM, PGA450-Q1

Hi Team,

Do you have transducers list that is usable with PGA450Q1EVM?
My customer wants to evaluate with different transducers with EVM.

If the answer is no, I believe the transducer that meets the following is usable.
Is my understanding correct?
---------------------------
drive voltage: 94 to 160Vpp (with default transformer of EVM)
transducer frequency: 40-70kHz
---------------------------

Best Regards,
Yaita / Japan disty

  • Hello K.Yaita,

    An alternative to the Murata MA58MF14-7N is the K-Series selection from SensComp (www.senscomp.com/.../piezoelectric-sensors.php). Otherwise, as long as the chosen transducer meets the specifications you've listed, it should be compatible with the PGA450-Q1.
  • Hi Akeem-san,

    Thank you for your support, however I coudn't access the link you attached.
    Could you confirm it?

    Best Regards,
    Yaita

  • I would like to ask one more..
    My customer wants to detect the target object with long distance and surgical precision (narrow vertical and narrow horizontal directivity).

    I believe he should change the transducer from default MA58MF14-7N (Murata) to another.
    Is my understanding correct?
    Do you recommend my customer to have a talk with transducer vendor to select appropriate transducer?

    Best Regards,
    Yaita

  • Hi Yaita,

    Sorry if the link does not work. If you are able to perform a web search for "SensComp", navigate to their Ultrasonic sensors --> Piezoelectric Ultrasonic Sensors --> K-Series or L-Series. I recommend having the customer contact them at info@senscomp.com to discuss which transducer may be most appropriate.

    For the majority of open-air ultrasonic applications,  transducers typically operate in the frequency range of 30kHz to 450kHz. As frequency increases, the attenuation of sound waves in the air increases. See the following relation: ↑ Frequency :: ↑ Resolution :: ↑ Narrower Directivity :: ↑ Attenuation :: ↓ Distance

    I recommend the SensComp 40KPT25, which has both a narrow vertical and horizontal beam pattern due to its wide top diameter. Alternatively, the MA58MF14-7N may have a narrow vertical and wide horizontal beam pattern, but the customer can use a horn to force focus the ultrasonic energy in a single direction. The horn approach is applicable to any transducer.