Hello,
We are using the PGA411 with a 2 poles resolver and the ABZ interface to the microcontroller.
There is one register DEV_CONFIG1 that has the NPLE bits. Those bits can be configured for 1x, 2x, 3x and 4x poles. Is that the number of poles of the emulated encoder output or the number of poles of the resolver?
Right now I have it configured as a 1x pole and because of the 2 poles resolver I get two index flags per rev so I would like to have just one, is this possible?
Regards,