To evaluate TPIC8101, we ordered a TPIC8101EVM board. We could run the GUI and set parameters using SPI. However, the EVM board did not seem to generate the 8Mhz clock, neither did it send the INT signal. We thought we bought a defective board we so we ordered another one from TI store, it behaved the same way. We then switched to a different computer to run the GUI, same result.
We did remove the hex jumper. All other jumpers are at default positions.
One thing we noticed, according to the EVM user guild, the default SPI mode should be normal. However, the echoed back data reflected the previous command instead of the current one.