Other Parts Discussed in Thread: TPS7B7702
Hello.
I'm trying to sale of TPS7B7702, now.
And I have a question about this product.
(I'm asked by this customer for this thing.)
So, please teach me about this thing.
<Question>
Junction temperature (Tj) of absolute maximum rating: - 40 to 150 ° C and ambient temperature (TA): - 40 to 125 ° C.
However, Thermal shutdown detection temperature of this product is 175 ° C @ TYP (Junction).
In such a condition, I think that the detection temperature of Thermal shutdown is 150 ° C @ TYP and it is necessary to have hysteresis of about 15 ° C.
(This is because there is concern that "If the ambient temperature has reached near the rated rating, it is not reset if the IC is detected at 175 ° C.")
Is my consider a mistake?
Could you help us?
Best Regards,
Masumi Sekiguchi