Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA411-Q1: Problem reading angles and velocities from a 3-pole resolver

Part Number: PGA411-Q1

Hi!

I am trying to interface a PGA411-Q1 to a 3-pole resolver via the PGA411-Q1 EVM development board.

The problem is, that whatever values I set in the DEV_CONFIG1 / NPLE register, I always read a velocity that is three  times too high, and when I move the resolver through 360°, I get three cycles of 0-359°, instead of just one.

Why is the PGA411 seemingly ignoring the NPLE register?

Best Regards

Anthony Robertson.