Hello,
One of my customers want to implement buck-boost converter as on EVM.
Where can I get TPIC74100 EVM gerbers?
Please attach here or e-mail me. My e-mail id is sanjayrpithadia@ti.com
Thanks for the help!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
One of my customers want to implement buck-boost converter as on EVM.
Where can I get TPIC74100 EVM gerbers?
Please attach here or e-mail me. My e-mail id is sanjayrpithadia@ti.com
Thanks for the help!!
Hello,
Is it possible to use TPIC74100-Q1 for output voltages other than 5V?
I could not locate this information from the datasheet.
Thanks.
The output voltage feedback resistor string in internal, so this would have to be changed. The internal logic runs off of the output voltage and this has an absolute maximum of 6V. All of the simulation and evaluation has been done for a 5V output voltage. So, it is possible to increase the output voltage with design changes, but they would be more difficult than changing a resistor.
Thanks Tom!!
If I understand correctly, the changes are required from TI side. But with this device customer can not change the output voltage, as they will not be able to change the internal resistor string or internal logic. Right?