This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Change Real Screen Resolution



Hi,

I'm trying to use a 5.7" LCD screen with Beaglebone Black. I connected the pins and it's working but there is a problem. LCD's resolution is 640x480 and doesn't have an EEPROM. So Beaglebone is setting itself to its defualt resolution, which is 1280x720. I'm trying to change the resolution with:

am display-size 640x480

But it doesn't realy change the resolution. It just configure the resolution to look like a 640x480 in a 1280x720 screen. When I look at dumpsys with:

dumpsys window

it gives me:

DisplayContents:

Display: mDisplayId=0

init=1280x720 160dpi base=640x480 160dpi cur=640x480 .......

I think I need to change that init value. I think  that value is being set by communicating with LCD's EEPROM. Because when I connect a LCD3 Cape dumpsys window gives init=320x240. Or if LCD doesn't have an EEPROM Beaglebone set itself to its default resolution. I need to change that default resolution. Is there a adb or shell command I can use? Or should I change something in kernel?