This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DHCP/BOOTP: Ignoring delayed packet



 

I found an earlier posting with a similiar error. The resolution was not within the discussion. This is a copy of the email I received after I added to the old posting.

Bob Simning65205 replied to Re: OMAP3530EVM NFS File System Fail in Linux forum.

How did this ever get resolved? I am experiencing the same error with the C6A816x evaluation board.

 I had been using the evaluation board previously on a large network w/o issues.  We changed into a smaller network and I also moved my office network behind a small router to prevent my work from conflicting with the office network. Now when I try to load my NFS share I get the "DHCP/BOOTP:  Ignoring delayed packet" error.

This is my environment:

TI8168_EVM#printenv
verify=yes
ramdisk_file=ramdisk.gz
loadaddr=0x81000000
script_addr=0x80900000
loadbootscript=fatload mmc 1 ${script_addr} boot.scr
bootscript= echo Running bootscript from MMC/SD to set the ENV...; source ${script_addr}
ethaddr=90:d7:eb:95:95:32
ethact=DaVinci EMAC
bootdelay=4
baudrate=115200
autoload=no
oldbootfile=uImage
bootfile=uImage-dm816x-evm.bin
bootargs=console=ttyO2,115200n8 rootwait rw mem=256M earlyprintk vram=50M ti816xfb.vram=0:16M,1:16M,2:6M root=/dev/nfs nfsroot=192.168.1.100:/home/c6A186x/targetfs ip=dhcp
serverip=192.168.1.100
bootcmd=dhcp;setenv serverip 192.168.1.100;tftpboot;bootm
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2010.06 (Jun 01 2011 - 12:30:57)

 

Any suggestions?

 

  • A very old thread, but this shows up higher in google results than others.  In http://e2e.ti.com/support/embedded/linux/f/354/t/154681.aspx Anil Kumar points to http://e2e.ti.com/support/embedded/linux/f/354/t/127289.aspx which says in sum, "the dhcp server answering queries is not providing sufficient information in the reply, use another".