HI,
We are thinking about using keystone 1 along side of another processor. We don't know yet whether it is going to be arm or x86 but We would like to take advantage of Syslink to communicate between the GPP because it is flexible and mature.
In order to start developing and experimenting, I would like to use my EVM 6678 board connected to a standard linux box using PCIe.
Can someone tell me if it is possible to build syslink to run on a standard linux box (or eventually on a non-TI ARM processor) ?
And if yes, is there any documentation on how to build it and have to right linux driver to use it ?
Thank you
PS. I looked at the source taken from linux-c6x-2.x.. and it does not seem to support standard linux target