This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ERROR: can't get kernel image

Other Parts Discussed in Thread: DM3730, SEGGER

Hi,

I am having a big problem with my Gumstix board.

When I turn on my Gumstix board, the executions stops after the boot timeout:

OMAP36XX/37XX-GP ES2.1, CPU-OPP2, L3-165MHz, Max CPU Clock 1 Ghz
Gumstix Overo board + LPDDR/NAND
I2C:   ready
DRAM:  512 MiB
NAND:  512 MiB
MMC:   OMAP SD/MMC: 0
In:    serial
Out:   serial
Err:   serial
Board revision: 1
Tranceiver detected on mmc2
No EEPROM on expansion board
Die ID #248c00029ff80000015913d805007022
Net:   No ethernet found.
Hit any key to stop autoboot:  0
Booting from nand ...

NAND read: device 0 offset 0x280000, size 0x400000
 4194304 bytes read: OK
## Booting kernel from Legacy Image at 82000000 ...
   Image Name:   Angstrom/2.6.34/overo
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3160052 Bytes = 3 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
Overo #


I tried to insert the SD card in order to restore the whole system but it does not work.

It seems impossible to read any data from the SD card. How can I solve my problem ?

These are my environment variables for uBoot, and it always worked for me.

baudrate=115200
bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi
bootdelay=5
bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
console=ttyS2,115200n8
defaultdisplay=dvi
dieid#=248c00029ff80000015913d805007022
dvimode=1024x768MR-16@60
loadaddr=0x82000000
loadbootscript=fatload mmc ${mmcdev} ${loadaddr} boot.scr
loaduimage=fatload mmc ${mmcdev} ${loadaddr} uImage
mmcargs=setenv bootargs console=${console} mpurate=${mpurate} vram=${vram} omapfb.mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} root=${mmcroot} rootfstype=${mmcrootfstype}
mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
mmcdev=0
mmcroot=/dev/mmcblk0p2 rw
mmcrootfstype=ext3 rootwait
mpurate=500
nandargs=setenv bootargs console=${console} mpurate=${mpurate} vram=${vram} omapfb.mode=dvi:${dvimode} omapdss.def_disp=${defaultdisplay} root=${nandroot} rootfstype=${nandrootfstype}
nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000 400000; bootm ${loadaddr}
nandroot=/dev/mtdblock4 rw
nandrootfstype=jffs2
stderr=serial
stdin=serial
stdout=serial
vram=12M


I don't know how to proceed..

Could be helpfull to reflash the microprocessor with the ARM JTAG ?

Thank you in advance for your help.
Simon