Hi, im new here and am really in need of some help. I have a standalone cctv dvr (intellix anf1648) unit thats running an embedded monte vista linux pro 4.0.1. its a da-vinci based platform DM6467. Im connected to it via serial (rs232) port and have it connected to my laptop, which is on windows using PuTTY. ive got the terminal settings correct and i get output from the console. Im trying to figure out how to stop the autoboot process. it says "press any key to stop autoboot" and ive tried control+c and everything else i can think of and it seems as if the unit isnt accepting commands until after the kernel has been loaded. which is past the point of stop autoboot.