Hello,
I want to use OMAP timers with Linux, Is there any example for this ?
I've searched, but did not found any.
Thank you,
Ran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ran,
In addition to Titus' post, I suggest you taking a look on the wiki - http://www.omappedia.org/wiki/Timer
http://lxr.free-electrons.com/source/Documentation/devicetree/bindings/arm/omap/timer.txt
http://lxr.free-electrons.com/source/arch/arm/plat-omap/dmtimer.c
http://lxr.free-electrons.com/source/arch/arm/mach-omap2/timer.c
Best regards,
Yanko
Hi,
We are using OMAP3530, with SDK :

I think that the driver you've given is not relevant.
I think the HW timers are named in OMAP as "GP timer" (= dmtimer).

I try to see if there is any example how it is used, but didn't find. I guess I'll need to delve into the GT driver code...

Thanks,
Ran
Hi Titus, Yanko,
Thank you for the information source.
Yet, I seem to be missing the understanding of how to use these HW timers.
1. Does anyone knows what is the difference between the GT timer to DM timer. It seems that there are 2 interfaces, and that the GP timer uses DMtimers.
2. If I build some kernel module which uses HW timers, should I use the dmtimers interface or better use GP timers ?
Thank you,
Ran
Hi,
I see also the example of using GP timers with DM814x, DM816x

But I would like to ask how I can check which timers ID are available for use in kernel ?
or maybe it is just better to use
omap_dm_timer_request()
instead of
omap_dm_timer_request_specific() ?
Thank you,
Ran