Other Parts Discussed in Thread: TMS320DM355
Hi all
Please tell me if there is any driver available for Aptina's MT9M112 camera board, so that I can use it with LeopardBoard 355.
Thanks and regards.
Bhagat Singh Rajawat
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320DM355
Hi all
Please tell me if there is any driver available for Aptina's MT9M112 camera board, so that I can use it with LeopardBoard 355.
Thanks and regards.
Bhagat Singh Rajawat
Bhagat,
Beagle board community is actively involved in developing camera support, the validation code at gitorious has been tested to work with the beagle-xM camera module. Which processor/EVM do you plan to use?
Validation code at: http://gitorious.org/beagleboard-validation/linux/commits/validation-20100805
Thanks, Punya
---------------------------------------------------------------------------------------------------------
Please
click the Verify Answer
button on this post if it answers your question.
---------------------------------------------------------------------------------------------------------
Sir, I am using Leopardboard 355 which uses TMS320DM355 processor board from TI.
The camera module is 1.3 Mega pixel camera board from Leopard Imaging, which uses Aptina's 1/4" CMOS sensor SoC MT9M112.
Thanks for guidance.
Bhagat Singh Rajawat