This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: cannot get LCD to work

Part Number: PROCESSOR-SDK-AM335X


Tool/software: Linux

hi.

we have a board based on am335x, for which we have used ti-sdk-am335x-evm-07.00.00.00 for developing software. the lcdc settings in the dts file, which is a copy of those in am335x-evm.dts apart from display_timings worked fine. (dts_lcd_orig.txt)

6708.dts_lcdc_orig.txt

we have decided to update the software, so, switched to /ti-processor-sdk-linux-rt-am335x-evm-04.00.00.04. though the dts did not compile well, so, we have restructured it to be similar to the am335x-evm.dts in this new SDK. however, there is no activity on the display (except from the backlight): no boot logo (CONFIG enabled), no terminal. the kernel messages are:

[    1.163806] [drm] Initialized
[    1.167976] panel panel: found backlight
[    1.173004] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    1.179664] [drm] No driver support for vblank timestamp query.
[    1.185983] tilcdc 4830e000.lcdc: No connectors reported connected with modes
[    1.193180] [drm] Cannot find any crtc or sizes - going 1024x768
[    1.217403] Console: switching to colour frame buffer device 128x48
[    1.234145] tilcdc 4830e000.lcdc: fb0:  frame buffer device

i followed the Linux Core LCD Controller user guide, but it does not work. can someone advice?

thank you.

8156.dts_panel.txt