This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-OMAPL138: ubi_ctrl missing ? / OMAPL138-Linux

Part Number: PROCESSOR-SDK-OMAPL138

Tool/software: Linux

My sdk is 'PROCESSOR-SDK-LINUX-OMAPL138  04_00_00_04'.

I want to use 'ubifs filesystem'.

I made ubi-image and ubiformat.

But, when ubiattach, get massage "ubiattach: error!: UBI is not present in the system"

----------------blow1 ---------------------------------------

root@omapl138-lcdk:~# flash_eraseall /dev/mtd3

flash_eraseall has been replaced by `flash_erase <mtddev> 0 0`; please use it

Erasing 128 Kibyte @ 1fec0000 -- 99 % complete flash_erase: Skipping bad block at 1fee0000

flash_erase: Skipping bad block at 1ff00000

flash_erase: Skipping bad block at 1ff20000

flash_erase: Skipping bad block at 1ff40000

Erasing 128 Kibyte @ 1ff40000 -- 100 % complete

root@omapl138-lcdk:~# ubiformat /dev/mtd3 -f system.ubi -s 2048 -O 2048

ubiformat: mtd3 (nand), size 536215552 bytes (511.4 MiB), 4091 eraseblocks of 131072 bytes (128.0 KiB), min. I/O size 2048 bytes

libscan: scanning eraseblock 4090 -- 100 % complete

ubiformat: 4087 eraseblocks are supposedly empty

ubiformat: 4 bad eraseblocks found, numbers: 4087, 4088, 4089, 4090

ubiformat: flashing eraseblock 1118 -- 100 % complete

ubiformat: formatting eraseblock 4090 -- 100 % complete

root@omapl138-lcdk:~# ubiattach /dev/ubi_ctrl -m 3 -O 2048

ubiattach: error!: UBI is not present in the system

---------------------------------------------------------

I checked related files like blow.

ubi_ctrl & /sys/class/misc/ubi is not.

----------------------blow2-------------------------------------

root@omapl138-lcdk:~# ls /dev/u*
/dev/udev_network_queue  /dev/urandom
root@omapl138-lcdk:~# ls /sys/class/misc/
autofs              cpu_dma_latency     crypto              memory_bandwidth    network_latency     network_throughput  watchdog

-----------------------------------------------------------

Kernel option of ubifs is ok.

1) Device Drivers --->
     Memory Technology Device (MTD) support  --->
         Enable UBI - Unsorted block images  --->

2) File systems  --->
     Miscellaneous filesystems  --->
          UBIFS file system support

3) Device Drivers -> 
      Generic Driver Options ->
        Maintain devtmpfs

How to add ubi_ctrl & sys/class/misc/ubi ?

Thanks.