Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hi,
I want to run application that uses graphical accelerator but it fails saying there are issues finding EGL library.
I used SDK 03.03 to build the kernel and file system. The file system used is arago-base.
I also built and installed to the file system ti-sgx-ddk-km package, which is available from the sdk top level make.
It looks like this is only the physical layer driver, and for an application to use accelerator I need user space libraries.
I used bitbake to compile ti-sgx-ddk-um, which is not available from the SDK top level make.
When trying to install these libraries I only managed to install dbg and dev packages
The other two fail the dependencies check:
* satisfy_dependencies_for: Cannot satisfy the following dependencies for ti-sgx-ddk-um:
* wayland (>= 1.9.0) * libdrm-omap1 (>= 2.4.67) * libgbm2 (>= 10.0.0) * ti-sgx-ddk-um-plugins *
* opkg_install: Cannot install package ti-sgx-ddk-um
Is the libEGL part of the ti-sgx-ddk-um driver package?
And if so do I need wayland installed for it?
I struggle to find documentation on how to install and set up drivers required for an application to use 3d accelerator.
Kind regards,
Ugnius