This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

make distclean fails



(Please be sure to see P.P.S. at bottom)

I'm following the instructions at http://processors.wiki.ti.com/index.php/Linux_Toolchain#Kernel

When I try the command "make distclean", it doesn't work.  At first, I got an error about no rule for distclean.  I immediately recognized that I had to change the working directory to the folder containing the tar extraction (this needs to be added to wiki above).  Next, the first output from "make distclean" is:

Makefile:314: /<snip>/linux-davinci-b411b51/scripts/Kbuild.include: No such file or directory

where <snip> is the long pathname to where I've extracted the tar.

Note that "ls" provides

arch  block  COPYING  CREDITS  crypto  Documentation  drivers  Kbuild  Kconfig  MAINTAINERS  Makefile  README  REPORTING-BUGS

and there is no "scripts" folder in the tree.  Is my problem indeed that the "scripts" folder is missing?  I downloaded the tar from git.kernel.org with Internet Explorer according to the "git snapshot" instructions a little higher in the same link I first referenced above.  I believe the "b411b51" in the folder name above should sufficiently identify WHAT I downloaded. 

Note that I'm running ubuntu under vmware under WIndows XP.  The <snip> folder is on a share living on my Windows XP machine, and I used IE to download the tar to this folder.  I unzipped the tar from Windows XP.  Within ubuntu terminal I changed working directories to this shared folder.

Thanks very much,

Helmut

P.S. I get a similar Makefile:314 error trying the subsequent make commands from the wiki link, each error including scripts/Kbuild.include, so it's not just distclean that fails, but everything.  I'm thinking this must really be about scripts missing.

P.P.S. Doing some searching, I find in my DVSDK that came with DM6467T EVM a file linux-davinci-staging.tar.gz.  Inside I find a bunch of source code and folders similar to those in my <snip> folder.  I'm thinking this tar contains the stuff to remake the existing kernel for my DM6467T EVM.  What's best is that I see a "scripts" folder in there.  I'm thinking I should forget my <snip> folder and start again from this tar...  What do you think?