Hi,
I have a F2812 project that was building fine and also debugging with CCS6 using DSP/BIOS 5.49. I could open the tcf file in the config tool and edit, and build the project without any problems. Now, without any changes to the tcf file, I get an error when building that I traced to the tcf file being unable to open with the config tool. Here is the error when opening the tcf file:
Unable to create BIOS config server.
And the error when building the project is:
Buildfile generation error occurred..
Cannot build project. Referenced project 'SingenX05-3a' contains build-errors.
Build stopped..
In the Problems view, I get an error: gmake error 1, which I think is just saying it can't build the project, but it's not really saying why. I'm fairly sure it's due to not being able to open the tcf file. Also, while troubleshooting this an hour ago, I was getting a slightly different build error: "can't create session manager: create of JVM failed".
I've looked at some related posts and wikis but I'm stumped on this. I even tried re installing CCSv6.1.0, although I didn't uninstall first.
I know that there's nothing wrong with my tcf file as I just moved the project yesterday from CCSv5.5 to CCSv6.1.0 and copied over the tcf file along with the rest of the project to my new CCS6 workspace. In case I did mess up the tcf, I recopied the original CCSv5 version into the CCS6 project and there is no change in the result.
Please help as I'm completely stumped. Thanks.