Hello,
We have an extended handle object for our codec engine:
typedef struct OUR_ALGORITHM_Obj
{
IALG_Obj alg; /* MUST be first field of all XDAS algs */
IDMA3_Handle dmaHandles[ MAX_DMA_HANDLES ];
void *memSegments[ MEM_NUM_SEGMENTS ];
int iDummy;
int iDummy2;
| |
int iDummyn;
}
OUR_ALGORITHM_Obj;
If we do the following in OUR_ALGORITHM_initObj():
OUR_ALGORITHM_Obj ourAlgorithmObj;
memset(&ourAlgorithmObj, 0, sizeof(OUR_ALGORITHM_Obj));
The codec crashes on the DM6446.
I figure something in the structure is filled in before OUR_ALGORITHM_initObj(), either the IALG_Obj at the start or the IDMA3_Handle array by OUR_ALGORITHM_dmaInit().
Could anyone explain this?
Thanks,
Matt