Hello,
I'm currently developing a RF solution using the CC1110 and for the purpose of the proyect it is needed to measure the distance between two devices in a P2P connection. My first thought was measure the time between the moment the connection is stablished and the first message is receved, and then convert this into distance but the accuracy is really poor.
Is there a method to measure the distance between two devices using the SimplicTI libraries?
Or has anyone measured the distance between two devices and has a sugestion of wether between which two processes measure the time in a connection?
I'm currently developing in IAR Embedded Workbench 7.60.