Other Parts Discussed in Thread: CC1101
Hello,
I'm testing the output of the CC1101 with a spectrum analyzer. My data rate in SmartRF is set to 153.13kBaud. When sending packets I can demodulate properly with a symbol rate of 153.13kHz, as expected. However, when sending in continuous modulated TX mode (which I'd like to use to develop a custom demodulator) I can only demodulate the stream when I have set a symbol rate of 9.6kHz on the spec an, despite the data rate in Smart RF still being set to 153.13kHz. Otherwise I just get junk.
Why is the continuous TX sending at a different data rate? Is there a way I can force the CC1101 to send a stream of 1's or 0's at a data rate besides 9.6kBaud?
I'm using GFSK modulation.