Hello e2e community,
I am looking for a table of DC Characteristics for the CC2540 when VDD is less than 3V. I am particularly interested in DC Characteristics when VDD = 2.1V
Section 7.2 of the user guide points to the datasheet for characteristics at lower VDD voltages.
"In applications where the digital I/O power supply voltage pins, DVDD1 and DVDD2, are below 2.6 V, the register bit PICTL.PADSC should be set to 1 in order to obtain the output dc characteristics specified in the DC Characteristics table in the device data sheet (Appendix C)."
Meanwhile the datasheet only references dc characteristics at VDD = 3V. http://www.ti.com/lit/ds/swrs110b/swrs110b.pdf
thanks in advance
-Ray