Other Parts Discussed in Thread: MSP430F2274, CC2530
Hello,
Our compnay wants to design a big PCB which contains the CC2530 processor (+ Antenna) and the MSP430 microcontrolleur (MSP430F2274).
Well, our PCB is a standard one (2 layers PCB), but I found that the target board of the CC2530_ZNP is a 4 layers one.
Did the CC2530_ZNP work with a two layer board or no? or I have to use a 4 layers one?
Also, is there another way to flash the CC2530 and MSP430 processors without using the USB part of the Zigbee, because in our board we will not integrate the USB part.
Regards,