Hello!
I am currently working on a new design for a customer and are developing a radio transciever unit. The unit is supposed to be able to transmit and recieve data with at least 57,6 kHz and the line of sight range requirement is 1000m. We have development kits of the CC1120 transciever and are quite happy with the test results. There is an existing solution today that uses the CC1101 transciever in combination with the CC1190 range extender but this solution is too sensitive to interference and the customer does not use the wireless module because of that.
So my question is if the CC1120 transciever will be better and more insensitive to interference compared to the CC1101? Or what is the main differences between the CC1101 and the CC1120 transcievers?
I also wonder if the CC1190 range extender can make the solution more sensitive to interference? The range of the CC1120 transciever is fine without the CC1190 so is there a reason to use the range extender?
Hopefully someone can help me.
/ Mikael